Hi!
Since there is no category about playing/working with the Intel embedded boards, I post my question here.
I want to run Node.js on an Intel Galileo but I get stuck building the SD Card. I am trying to follow the different manuals.
-
I formatted the SD card with an FAT32 filesystem. But booting that one was not working.
-
Formatting the card with an ext3 filesystem made the content readable, but the SD Card was neither bootable.
All I see is the boot menu which looks like below. Then the SPI Flash is booted again.
GNU GRUB version 0.97 (604K lower / 244604K upper memory)
±------------------------------------------------------------------------+
| ---- No “boot/grub/grub.conf” file found on 1st USB or SD device ---- |
| Clanton SVP kernel-SPI initrd-SPI IMR-On IO-APIC/HPET NoEMU |
| Clanton SVP kernel-SPI initrd-MassStorage big-rootfs IMR-On IO-APIC/H> |
| Clanton SVP kernel-MassStorage initrd-MassStorage small-rootfs IMR-On> |
| Clanton SVP kernel-MassStorage initrd-MassStorage big-rootfs IMR-On I> |
| Clanton SVP kernel-MassStorage initrd-MassStorage big-rootfs IMR-On I> |
| |
| |
| |
| |
| |
| |
±------------------------------------------------------------------------+
Use the ^ and v keys to select which entry is highlighted.
Press enter to boot the selected OS, ‘e’ to edit the
commands before booting, ‘a’ to modify the kernel arguments
before booting, or ‘c’ for a command-line.
Error 5: Partition table invalid or corrupt