Hi,
I recently purchased an UM96 which I for starters am trying to interface with my Bus pirate.
My pin setup is like this:
Pin 1 connected to bus pirates ground
Pin 2 to bus pirates 5v
pin 3 not connected
pin 4 not connected
pin 5 to pirates ground
pin 6 to pirates mosi
pin 7 to pirates miso
pin 8 not connected
pin 9 to bus pirates 5v
I have only jumper D connected.
Interfacing with the pirate I am choosing UART mode, 9600, 8N1, Idle 1, Normal output type (Normal (H=3.3V, L=GND)).
I am powering it on, and listening for data with the pirate command W(2).
As far as I understand I should have seen a “boot message” from the UM96 saying something like “uM96v2.31AXM”, which I do not.
And I would have guessed I would see data by pointing a 433.92 remote sender at it.
I hope someone can help me with this.
Espen