Cable for GNSS Multi-Band L1/L2/L5 Helical Antenna

Hi. Looking at this product but do not see a link to a cable that would be used. The description includes a warning stating that a locking SMA connector is required. I plan to connect to this piHat.

Welcome @kbares! Sorry for the confusion - any SMA cable is compatible with that antenna. Here is our 10m SMA cable, 1m SMA cable, and 25cm SMA cable.

‘Locking’ means only that the antenna has additional screw holes in it so you, if you want, you can prevent people from simply rotating off the antenna from the SMA connection by putting in additional screws.

Thanks for clearing that up! Really appreciate it.

No problem! Happy to help.

Yeah the “Connector-Type Notice: Please be aware that this GNSS Antenna is equipped with a locking SMA connector! It cannot be simply unscrewed like a normal SMA-type.” in the bold alert box does seem super unhelpful. Implies some kind of locking nut, or thread machining, that only allows for tightening.