My Facet is stuck without wifi and Terra Term will not connect as well.
In Terra Term the only repeating msg i get is: “Halted: network user PVT UDP server is already idle”
I think i misspelled my wifi password before this happened as well so i cant connect to it at all. It also wont turn off with the button. I have let the battery run out, recharged, and then have the same problem.
The facet display says; " ssid rtk config IP 192.168.4."
i don’t think it’s just the wifi password. Terra sync doesn’t connect either. And although the facet shows the Bluetooth on the screen, SW maps will not display any data in the bottom of the screen and my phone does not show connection to the facet.
When i set facet to Configure screen the unit completely freezes up and i have to let the battery die to restart.
In Terra Term the only repeating msg i get is: “Halted: network user PVT UDP server is already idle”
i used the gui to go back to firmware 3.10rc, then upgraded back to 4.0 again. Still have the freezing issue when in config mode. but it does Bluetooth connect to sw maps now.