devpts
November 27, 2012, 10:37am
1
I bought and mounted the [Chip scale GPS Antenna .
1.575Ghz VSWR is 1.3 with with return loss at 18.6dB.
Center frequncy as mounted is 1.58Ghz with VSWR at 1.2 and return loss is 20.16dB
Problem: several GPS devices fail to acquire initial data: no position
Solution: Connect alternate antenna for initial fix, remove and connect chip antenna for all subsequante fixes
Questions:
What might cause the inital failure
How might this be corrected](Antenna GPS Chip-Scale - GPS-09131 - SparkFun Electronics )
You are not getting enough signal with the chip antenna.
devpts
November 27, 2012, 3:55pm
3
leon_heller:
You are not getting enough signal with the chip antenna.
This doesn’t make sense as the antenna works fine for subsequent updates.
It just does not work for cold start.
According to the description provided by SparkFun:
the gain is not as great (to be expected), but heck, if you can get a lock with this little guy, who cares?
That is a pretty big "if".
gm
November 27, 2012, 6:41pm
5
devpts:
This doesn’t make sense as the antenna works fine for subsequent updates.
This confirms that the signal is weak as a GPS usually requires a stronger signal to acquire the position and can track a weaker signal. If you look in the specs of the GPS you will notice something like
Tracking Sensitivity -160 dBm
Acquisition Sensitivity -148 dBm
Hope this help,
gm