Hello everybody!
I’m having this problem… I buy a MG-S01SP SiRFstarIII Module and I can’t get valid GPS position.
This module has an internal antenna.
I 've connected the power supply (3.3v), the Vbat also to 3.3v and Reset with a Pull-Up resistor also to 3.3v.
Then I have a LED in the GPS Status pin (the manual says that this LED will blink when GPS is fixed otherwise it will remain on) . And finally the Tx/Rx signals with a MAX232 to the PC.
I’m at the balcony, and I turn it on… The LED (GPS Status) lights up. And I get invalid position (I see it in the PC)…
Then SOMETIMES the LED begin to blink, so it means that at least find 1 satellite so it’s syncronized… at least that is what I understand for “GPS fixed”
And invalid data keep coming… And only ONE TIME I get valid position… I’ve done several test and never again get valid position… Sometimes the LED doesn’t even blink.
I don’t think that it’s a matter of visibility with the sky because I’m at the balcony and there is plenty of sky, lol…
I wonder if it could be the internal antenna… Because since I’m just doing some tests I plug it to a proto-board… So the proto-board my interfere… But the manual says it has high sensitivity: -159dBm
Another thing that I notice is that the datasheet says that in cold start the Acquisition Rate is 42 sec average… I’ve waited minutes and nothing…
Any suggestion? Please help!!! ANYTHING!!! ![]()