In my last post I had calculated Vout of an op amp according to its common/differential mode gains which was:
Vout = A_cm * V_cm + A_d * V_d
Vout = -1.13.5V + 1.453V
Vout = -3.85V + 4.35V
Vout = 0.5V
I am reading up on the CMRR of an op amp. And I Quote:
However, in real amplifiers there is always some variation and the ratio of the change to the output voltage with regards to the change in the common mode input voltage is called the Common Mode Rejection Ratio or CMRR. Opamps typically have a CMRR of around 80 dB and the higher the better.
If we calculate the CMRR of my circuit I only get:
The choice of resistor values and their precision is a critical factor in optimizing the CMRR. After proper choice of their values, you need to use resistors with better than 1% precision and they are expensive. People usually buy differential amplifiers as a self contained unit (called an instrumentation amplifier) for just this reason. http://en.wikipedia.org/wiki/Instrumentation_amplifier
You had a circuit, that *used* an op-amp. Your circuit made no attempt to be a differential **ONLY** amplifier. It's neither good or bad, it is what it is. If you wanted a differential amplifier circuit, you'd have chosen the resistor values to be different from what they were. DId that circuit have any real intended usage ?
The choice of resistor values and their precision is a critical factor in optimizing the CMRR. After proper choice of their values, you need to use resistors with better than 1% precision and they are expensive. People usually buy differential amplifiers as a self contained unit (called an instrumentation amplifier) for just this reason. http://en.wikipedia.org/wiki/Instrumentation_amplifier