The wikipedia entry doesn’t seem to be a very helpful discussion and the example is not very useful. It deals only with an open loop op amp configuration.
Sure why not ? But do be careful to know what V+-V- is when the circuit uses the op-amp in a feedback configuration. Especially as the open loop gain is not a well specified parameter. It's just guaranteed to exceed some number at DC. Nobody can tell you a specific number for the gain as it'll vary from op-amp to op-amp, with temperature and supply voltage, etc, etc. I think you need to understand more about feedback before my answer will make much sense to you.
Gopenloop is the gain of the operational amplifier with no feedback and is typically 1,000,000 (10^6) or higher. If you know what it is for a particular op amp, then for a given output voltage Vout, you can calculate the voltage difference at the inputs (Vin+) - (Vin-), which is typically a few microvolts. This is what Mee_n_Mac was referring to in an earlier post.
8Volts:
yes but my numbers came from a circuit with feedback
Yes and that feedback pushes Vout so that the difference between V+ and V- (these are the voltages at the op-amp inputs) is very small. In fact the difference at those places in the circuit is proportional to the open loop gain of the op-amp, a number you won't know exactly in real-life. Note that the V+ and V- are not the inputs to the circuit, which is what you wrongly used in your post above. Also Ad of the circuit is not the open loop gain of the op-amp.