I’ve been playing around with compiling the RTK Facet (L-Band) source code, and I’m hitting a wall. Hoping someone could shed some light on the issue:
My goal is to modify the code to add an auto power on and auto power off feature. I’ve got that working, compiling, and uploading into RTK Facets fine, but the issue comes from the compiler not being able to build in the SparkFun PointPerfect token, and therefore never being able to commission the RTK correction service on the device in question. Here’s what I mean:
I’m using Arduino IDE 1.8.15 (or 2.1.0) on Windows 10 home 64bit, ESP core 2.0.2, all the appropriate libraries, partition file and settings, etc. – Following the compiling instructions here https://docs.sparkfun.com/SparkFun_RTK_ … #windows_1
This is from the most recent ver 3.3 of the code in RTK_Surveyor.ino, line 36:
//This is passed in from compiler extra flags
#ifndef POINTPERFECT_TOKEN
#define FIRMWARE_VERSION_MAJOR 99
#define FIRMWARE_VERSION_MINOR 99
From what I can tell, versions 3.1 onwards use compiler extra flags for version numbers and pointperfect tokens. All versions use compiler flags for pointperfect tokens.
I found the workflow yaml file, and realized that SparkFun is using a GitHub action and Arduino CLI to compile and release. – the last paragraph of the compile instructions says so:
“The firmware can be compiled using Arduino CLI. This makes compilation fairly platform independent and flexible. All release candidates and firmware releases are compiled using Arduino CLI using a github action…”
This is cool, but it’s that workflow file that’s defining both the revision number and pointperfect token: (near the top of the file)
FIRMWARE_VERSION_MAJOR: 3
FIRMWARE_VERSION_MINOR: 3
POINTPERFECT_TOKEN: ${{ secrets.POINTPERFECT_TOKEN }}
If the SparkFun pointperfect token is loaded in during compile time as a secret on SparkFun’s repository, how can I do a successful, offline compile?
This applies to unmodified I compile as well – I just noticed the issue first on my modified code.
Also, Sparky, if you’re reading: this is unrelated to the RTK float issue I’ve reported on in the past – all of those units are stock, unmodified code from released .bin files ![]()