Sorry for the late reply, I was out sick for the last two weeks (children as well).
I was able to test v2.5 firmware with L-Band today. It works fine for me.
I have the fix but without the 3 bars on the satellite icon.
This would indicate your unit is not receiving L-band signal or not successfully decrypting messages.
Would you please connect over serial and output the serial data that is seen during power up: https://docs.sparkfun.com/SparkFun_RTK_ … th_serial/
Below you can see the output from my unit.
rst:0xc (SW_CPU_RESET),boot:0x13 (SPI_FAST_FLASH_BOOT)
configsip: 0, SPIWP:0xee
clk_drv:0x00,q_drv:0x00,d_drv:0x00,cs0_drv:0x00,hd_drv:0x00,wp_drv:0x00
mode:DIO, clock div:1
load:0x3fff0030,len:1240
load:0x40078000,len:13012
load:0x40080400,len:3648
entry 0x400805f8
Display started
ZED-F9P firmware: HPG 1.32
LittleFS Started
SparkFun RTK Facet L-Band v2.5-Sep 21 2022
Reset reason: ESP_RST_SW
Profile ‘Profile1’ loaded
MAX17048 configuration complete
Batt (75%): Voltage: 3.98V Discharging: -0.21%/hr Green
GNSS configuration complete
Accelerometer configuration complete
NEO-D9S firmware: PMP 1.04
System time set to: Thursday, October 27 2022 16:08:14
State: Keys Days Remaining, 2022-10-27 16:08:14.055
Days until PointPerfect keys expire: 50
State: Keys L-Band Configure, 2022-10-27 16:08:16.232
Batt (75%): Voltage: 3.98V Discharging: -0.21%/hr Green
State: Rover - Not Started, 2022-10-27 16:08:17.280
Bluetooth broadcasting as: Facet L-Band Rover-8F9E
*NTRIP_CLIENT_OFF
State: Rover - No Fix, 2022-10-27 16:08:19.523
Batt (75%): Voltage: 3.98V Discharging: -0.21%/hr Green
State: Rover - Fix, 2022-10-27 16:08:25.561
Rover Accuracy (m): 199.3658
Batt (75%): Voltage: 3.98V Discharging: -0.21%/hr Green
Rover Accuracy (m): 54.2646
Rover Accuracy (m): 45.4240