I seem to be having this same issue. I appear to be running 2.2. I downloaded 2.6 and used the Windows GUI v1.5.2 to update to RTK_Surveyor_Firmware_v2_6.bin. But it does not seem to have taken effect… See outputs below
UPLOADER OUTPUT
ESP32 Flash Size Detection
Command: [‘–chip’, ‘esp32’, ‘–port’, ‘\\.\COM6’, ‘–baud’, ‘115200’, ‘–before’, ‘default_reset’, ‘–after’, ‘no_reset’, ‘flash_id’]
esptool.py v3.3
Serial port \.\COM6
Flash detection complete. Uploading firmware…
Flash size not detected! Defaulting to 16MB
Uploading firmware
ESP32 Firmware Upload
Command: [‘–chip’, ‘esp32’, ‘–port’, ‘\\.\COM6’, ‘–baud’, ‘115200’, ‘–before’, ‘default_reset’, ‘–after’, ‘no_reset’, ‘write_flash’, ‘-z’, ‘–flash_mode’, ‘dio’, ‘–flash_freq’, ‘80m’, ‘–flash_size’, ‘detect’, ‘0x1000’, ‘C:\Users\17703\AppData\Local\Temp\_MEI104562\resource\RTK_Surveyor.ino.bootloader.bin’, ‘0x8000’, ‘C:\Users\17703\AppData\Local\Temp\_MEI104562\resource\RTK_Surveyor_Partitions_16MB.bin’, ‘0xe000’, ‘C:\Users\17703\AppData\Local\Temp\_MEI104562\resource\boot_app0.bin’, ‘0x10000’, ‘C:/Users/17703/Downloads/RTK_Surveyor_Firmware_v2_6.bin’]
esptool.py v3.3
Serial port \.\COM6
Firmware upload complete. Resetting ESP32…
Resetting ESP32
TERMINAL OUTPUT
rst:0xc (SW_CPU_RESET),boot:0x13 (SPI_FAST_FLASH_BOOT)
configsip: 0, SPIWP:0xee
clk_drv:0x00,q_drv:0x00,d_drv:0x00,cs0_drv:0x00,hd_drv:0x00,wp_drv:0x00
mode:DIO, clock div:1
load:0x3fff0030,len:1240
load:0x40078000,len:13012
load:0x40080400,len:3648
entry 0x400805f8
ZED-F9P firmware: HPG 1.32
LittleFS Started
SparkFun RTK Facet L-Band v2.2-Jun 8 2022
Reset reason: ESP_RST_SW
Display started
Profile ‘Profile1’ loaded
MAX17048 configuration complete
Batt (97%): Voltage: 4.20V Charging: 9.78%/hr Green
GNSS configuration complete
Accelerometer configuration complete
System time set to: Tuesday, January 03 2023 19:48:51
State: Keys Needed
State: Keys L-Band Configure
State: Rover - Not Started
Batt (97%): Voltage: 4.20V Charging: 9.78%/hr Green
Bluetooth broadcasting as: Facet L-Band Rover-F976
State: Rover - No Fix
State: Rover - Fix
Rover Accuracy (m): 1.5179
Batt (97%): Voltage: 4.20V Charging: 9.78%/hr Green