I have an RTK Facet L-Band, product GPS-20000, that works great with one exception: I am not receiving satellite corrections.
Current state:
I can power on the Facet, it starts reading satellites as expected. After a few minutes it gets me to ~ 1 meter accuracy w/ 20-30 satellites. That all seems to work well. However, I never get any better accuracy - nor do the images on the Facet’s display indicate I am getting corrections (ie the 3 little bars on the satellite image).
Error:
Using Tera Term, I pull up the Main Menu, and then select System Status, which yields “L-Band: Online - Keys Good / Corrections Received Failed / Eb/N0[dB] <>9 is good): 0.00”.
…photo of this output is attached.
Historically what I’ve done:
-
Placed Facet in CONFIG mode (setup button presses until Config displays).
-
The Facet’s ESP32 boots into AP mode, and I successfully connect to WiFi
-
I successfully launched the webpage (192.168.4.1) and set the Home Wifi & pwd. I left the 3rd field blank under the PointPerfect section of the webpage.
-
I save and reboot.
-
The Facet successfully downloaded the keys, and I have 40 days remaining.
…everything seems to work as expected regarding key management.
Additional Test:
-
Via BT I connection my Android phone to the L-Band Facet.
-
Using SW Maps, i get a reading and everything works as expected at reduced accuracy.
-
I have an RTK Facet (non-L-Band version), product GPS-19984, so I thought I would using my account to send NTRIP corrections (as received from the cellphone) and that works perfectly…the system gets me to ~20mm accuracy. This tells me the L-Band Facet is capable of getting to RTK Fix, if it can just receive the corrections.
Current configuration:
Taken from the SFE_Facet_LBand_Settings_0.txt, the following configuration versions:
rtkIdentifier=34
rtkFirmwareVersion=v2.2-Jun 8 2022
zedFirmwareVersion=HPG 1.32
Conclusion:
The Facet L-Band is working at reduced accuracy, home WiFi is set, the keys are successfully downloading…BUT I never actually receive any corrections. I have left it on for over an hour, and still reduced accuracy.
I welcome any thoughts. I’m guessing I just need to return for a different one?
Thanks in advance.