HELLO!! I’m doing a school project with Lilypad! I have a question about connecting the simple lilypad board … and where I live I couldn’t get FT232 !! but I have a CP2102. I don’t know exactly how to connect it … any help is welcome! I made the following connection:
CP2102 has the next pins: DTR, RXD, TXD, + 5V, GD, 3V3
lilypad CP2102
DTR DTR
TX RX
RX TX
VCC +5V
GND -
GND GND
link to the the back part of the CP2102.
https://http2.mlstatic.com/D_NQ_NP_6940 … 020-O.webp
I saw an image that shows the connection to the lilypad with the FTDI 232 and I see that 1 pin of the GND of the lilypad is connected to the CTS of the FTDI but in my adapter the CTS is not a pin, it is a female “island” (in the picture looks better).
And the DTR pin of the lilypad is connected to the RTS pin of the FTDI232. A teacher tells me that it is ok if I connect the lilypad of the DTR pins with the DTR of my CP2102. I am so confused ![]()
greetings from Buenos Aires!