does anyone have a configuration file for Facet rtk firmware version 1.30 that works with the rover and can be configured and from the buttons on my Facet it came with firmware 1.13 and I want to go to 1.30 it seems much more stable I did tests with it but I can’t configure it from the facet button but only from Ublox Center. thank you
You will need to use u-center to update the firmware on the ZED-F9P. You can get more information here: https://learn.sparkfun.com/tutorials/ho … ceiver/all
The Facet uses an internal ESP32 to configure all aspects of the ZED-F9P. You should not have to use u-center to control the ZED. Please see the Facet Hookup Guide for more information about configuration: https://learn.sparkfun.com/tutorials/sp … -guide/all
I configured the messages from ublox, the problem is that I don’t know on which port it should be left in the ucenter so I can make the changes and from the web interface (192.168.4.1) I have firmware 1.12 installed for esp and whenever I try to check for example a constellation (glonas) after what I save the settings and the interface restarts back in the rover the constellation appears to me. I check the settings on 192.168.4.1 it appears unchecked but in my measurement program (surpad) the constellation appears visible, something what I didn’t suffer when I received gps Facet with the firmware 1_13 ublox si 1.10 esp
to uncheck a constellation, I think I made a grammatical mistake I am not a native English speaker, zed f9p are upgraded to firmawer 1.32 and i2c port in ucenter
to uncheck a constellation, I think I made a grammatical mistake I am not a native English speaker, zed f9p are upgraded to firmawer 1.32 and i2c port in ucenter
No problem! You are doing very well.
For the RTK series you should use the serial terminal configuration:
https://learn.sparkfun.com/tutorials/sp … l-terminal
or the AP Config over WiFi:
https://learn.sparkfun.com/tutorials/sp … ion—wifi
Using u-center to configure the message will not work. At every power on the RTK Facet will apply setting stored in the ESP32. If you make changes in u-center, they will be lost at the next power cycle.
Thanks for being right about the settings. the only thing I haven’t experienced is upgrading the firmware to turn off the receiver and see what happens and if it takes over the settings in esp