Hello All,
I have configured Xbee in API Mode.
PC : WIN XP SP3
XCTU : 5.3.8.6
Baud rate : 9600
COM Port : Serial COM1
“Test/Query” : OK
I am not able to Configure it with XCTU
Read/Write Modem : Failed to enter command mode
Error : Action Required Dialogue doesn’t disappear.
I want to change modem configuration & Program it with AT Mode.
Can you please help ?
Regards,
Vijay
waltr
2
Which XBee adapter board are you using? Give a link to the board so we know exactly which one you have.
Many do not work properly for updating XBee firmware since they do not have a RESET.
Search for “XBee firmware update” and “XBee Bricked” for more info of the issue and fixes.
This is really a duplicate post:
https://forum.sparkfun.com/viewtopic.php?f=13&t=37844
which you did not answer the questions asked.
I am using board from local company in india.
Please find following link :
ZIGBEE BASE BOARD RS232 : http://www.dnatechindia.com/Zigbee/Zigb … RS232.html
Hello Again,
I have checked again with another Xbee Base Module.
Test/Query is ok.
XCTU shows COORDINATOR AT Version - 1020 & ROUTER AT Version - 1220 in Modem Config
Reading Module parameters gives OK result in XCTU.
But, doesn’t show Modem Type,Function Set & Version.
Writing any value gives error : Getting modem type…OK
Programming modem…Lost communication with modem
Write Parameters…Failed.
Also, Terminal shows - Echo for any typed char.
Interesting info is that :
For 1st Xbee => LED Blinks 2 times per second (I think its Router)
For 2nd Xbee => LED Blinks 1 time per second (I think its Coordinator)
What can i check for communication in this 2 Xbee ?