Connecting to MSPF149 Using MSP-JTAG

My setup is as follows:

MSP430F149 Proto Board

MSP-JAP Parallel Port Programmer

Win XP

Olimex MSP Programmer

When I attempt Command > Read from the Programmer, it fails with the error message:

Cannot Initialize the Port

Reading Failed

Similarly, I also tried downloading code using the IAR compiler. It also failed when trying to connect to the proto board.

I noticed that the Olimex website had a link for drivers for the MSP-JTAG, but the link was broken. Am I missing a driver? Suggestions on where to download are appeciated.

Thanks, Brad

When all else fails, reboot the PC. Works fine now.