UPDATE: Solved. Problem was a defective cable. Leaving my steps here in case anyone ever runs into a similar problem.
I have 2 [MSP430-JTAG-TINY and 3 [MSP430P1611, recently bought from sparkfun. I have reproduced the following problem under both WinXP and Win7.
First I downloaded the latest Olimex drivers ([1.0.35) and the latest mspgcc ([2008-12-30).
Then I installed mspgcc and copied the complete set of Olimex DLL files (5) to the mspgcc\bin folder. That should be it, right? I reboot, for Windows’ sake. I always get this error:
C:\>msp430-jtag --lpt=USB
MSP430 JTAG programmer Version: 2.3
Use -h for help
Reset and release device...
An error occoured:
Could not reset target (no connection?): Could not communicate with FET
Now with the [Olimex Programmer Software 1.21 I get equally bad results. Of course I updated its DLLs with the ones from the update previously listed. Then I run it, select MSP430F1611 from the list, USB port, then hit “read”. It does something, because the LED turns off. But after a while, the program stops with “Cannot reseting device.” (sic).
After attempting to READ with the Olimex Programmer and closing the software, I get this error from msp430-jtag:
An error occoured:
Could not initialize the library (port: USB)
What am I doing wrong? The current driver is quite recent, has anyone else used it? I know I’m not TOO far because GDB seems to work. It identifies the device correctly.
C:\>msp430-gdbproxy --port=1000 msp430 USB
debug: MSP430_Initialize()
debug: MSP430_Configure()
debug: MSP430_VCC(3000)
debug: MSP430_Identify()
info:      msp430: Target device is a 'MSP430F1611' (type 42)
debug: MSP430_Configure()
notice:    msp430-gdbproxy: waiting on TCP port 1000
](http://www.olimex.com/dev/soft/msp430/MSPProg-121.zip)](GCC toolchain for MSP430 - Browse Files at SourceForge.net)](http://www.olimex.com/dev/soft/msp430/OLIMEX%20MSP430-DLL%20drivers%201.035.zip)](MSP430-P1611)](MSP430-JTAG-TINY-V2)