Hi,
some days ago I received the devel board with 430f1611 and the tiny jtag. I am trying to debug the small “blinking led” example and I cannot.
I installed cc2.0 and IAR kickstart, to check the behaviour. in IAR I simply get:
FATAL ERROR
Failed to initialize device.
Session aborted!
simple and quick…
CodeComposer shows me the gdb output trace:
Starting target server…
Could not initialize device interface
what am I doing wrong?
my config and progress:
the Olimex devel board with 430f1611 is powered by jtag tiny,
I installed the code composer first and after that I connected the jtag dongle it was detected I pointed to the Driver directory with Olimex driver, then copied the msp430.dll file (together with the three other to
{cc directory}\tools\targets\emulation\msp430\
then I found the blinking led example and wanted to check it out ![]()
the first time I managed to flash the device and the debuging started, probably the value I set the counter for the loop was to small because the led did not blink it was simply on. I terminated the debug and changed the value. the second time it was also not blinking (I found some examples where the value was 10000, and I set it to 50 and to 1000). during the third try I got the message…
I did not manage to access the device since then…
then I installed the kickstart and I also tried to run the gdb430 with the target config from CC. still the same.
I uninstalled and reinstalled the driver. the tiny is simetimes detected and sometimes not, I am not really sure if it is installed or not. I tried this on three computers, same result. even if it is recognized it does nothing.
I dont know if there are some fuses or locks I could activate/deactivate on the MSP. I did not touch any settings except those for TI usb fet, like already said in many posts before.
next week I will get the LPT jtag so I will try to check what is the reason the dongle or the board.
I really miss kind of manual for jtag tiny. for example at the beginning I noticed that the led is not only green, it was also a little bit red. What does it mean?
ok, hope this does not look to messy ![]()
any idea about what I did wrong is welcome.
krzysztof