Hello all,
I need some help setting up the above configuration.
I’m running Windows 2000, the JTAG-TINY is plugged into a USB port and into the JTAG connector of the MSP430F149 header board.
I installed “IAR Embedded Workbench KickStart for MSP430 V3”. Also installed the Olimex Jtag-Tiny driver, and copied the DLLs (msp430.dll + two others) to the Workbensh’s bin folder.
I built the “Flashing the LED” example.
If I go to Project → Options → FET Debugger in the ide, the “TI USB FET” Connection is set by default (without me selecting it), so I assume it was detected.
But when I want to download the program, I get the following error:
Sun Jan 29 15:59:32 2006: Failed to load debugee: D:\Programs\IAR Systems\Embedded Workbench 4.0\430\FET_examples\msp430x1xx\C-source\Debug\Exe\msp430x1xx (C).d43
And another questions: I also tried to download one of the examples (leds, modified) using mspgcc. That didn’t work either. When I do ‘make download-jtag’ I get this output:
msp430-jtag -e leds.elf
MSP430 parallel JTAG programmer Version: 2.1
Cleaning up after error…
Reset and release device…
An error occoured:
Can’t open interface
make: *** [download-jtag] Error 1
How exactly does Jtag-Tiny emulate the parallel interface ? Or is there a different way in mspgcc to download stuff through USB ?
Any help would be appreciated.