Hello,
Has anyone managed to locate the connector for the ET-202 GPS reciever.
I’m having quite a bit of trouble locating one.
Thanks
Robert
Hello,
Has anyone managed to locate the connector for the ET-202 GPS reciever.
I’m having quite a bit of trouble locating one.
Thanks
Robert
Your schematic?
Hi,
Schematic? Why do you need a schematic to source a compatible mating connector for that GPS module?
That connector is a 12 pin header with 1.27mm (0.05") pin spacing. These connectors are fairly common and can be sourced at places like Digikey and Mouser. You’ll need to order a piece of ribbon cable as well. Once you have the pieces, the mating connector simply crimps onto the end of the cable. I’d advise using an ohm meter to be sure you know which pins of the connector correspond to the individual wires at the end of the cable!
John
Greetings,
Here a picture with the cable connected to the GPS Receiver ET-202
https://www.facebook.com/photo.php?fbid … =1&theater
Best regards