Controlling LED Arrays on TCP/IP Networks Problems

Hi, I am using a LPC-E2124 Ethernet board and am trying to run the the sample code from the “Controlling LED Arrays on TCP/IP Networks” tutorial. I can succesfully download and run the example .hex file that is included with the source code, but when I attempt to recompile the project the .hex file I generate does not work. The blinking LED that should blink when the program is running does not run and the program can’t be communicated with the sample Java applet. I am using Rowely CrossStudio for ARM v1.6.