DataLogger Firmware 1.5.1 released

Hi All -

Version 1.5.1 of the DataLogger IoT firmware was just released.

Detailed are located on the release page.

The update is available via the Over The Air (OTA) option in the datalogger firmware, or loading off the SD Card. See the on-line documentation for more details.

Relese Notes:

  • Added support for the Garmin LIDAR-Lite v4 LED - Distance Measurement Sensor (Qwiic) sensor
  • Added support for the SparkFun Ambient Light Sensor - VEML6030 (Qwiic) sensor
  • Added support for the SparkFun Spectral UV Sensor - AS7331 (Qwiic) sensor
  • Fixed issue with auto loading some I2C addresses for the MCP9600 Thermocouple Amp device. All addresses should now work correctly
1 Like