does OLIMEX parrallel JTAG work with Keil uvision3 with LPC21XX series?
thanks for your reply but if you see http://hjtag.blogspot.com site
write:
H-JTAG supports SDT2.51, ADS1.2, RealView and IAR. With the help of H-JTAG, you can debug arm7/arm9 through wiggler or sdt-jtag.
in the list below there is no Keil.
is keil the same with Realview?
and in the My future plan page is listed below:
-
Update H-JTAG to support keil for arm;
-
Develop a free universial flash programmer;
-
Develop an USB in circuit emulator to improve the speed of H-JTAG;
so he tell that it doesn’t work with keil until now is it true?
hello
I use a board LPC H2129, under µVISION (Windows xp) and I wish to use JTAG.
I bought a cable JTAG from OLIMEX, but I do not arrive to detect the board using H-JTAG server.
I took the care to make all the verrifications but it always launches me the following message :
Unable to find target, please make sure that the hardwear is properly connected and powered up
it is the case,
thank you for all helps .
Hi,
you can use keil for arm + H-JTAG +Wiggler to debug LPC2000
in RAM, it can work well.But if you want to debug it in flash you
should first download the hex to your target board, after that
you can debug it. I have tyied it but it seem to have some bug
![]()
hi,
for downloading hex file can use flash programmer in keil or must use H-jtag flash programmer for lpc?
to nader:
I use H-jtag flasher to download hex file then
use keil to debug in flash. Still have some
problems, maybe my configuration of keil isn’t correct:(
in the last month i use iar flash debug for at91sam7.it’s really slow.now i want to switch to LPC2000.
i want to know is hjtag flash programmer faster than IAR flash loader?
if you have any success in keil please let me know.