DRC space fail

Hey guys, I am trying to get a pcb onto batchpcb and I am getting an error that I cant figure out.

Here is the error file

unmatched 274X paramblock OFA0B0 - len 6
Macro Name = OC8
Macro Consuming 5,1,8,0,0,1.08239X$1,22.5 [2]
PUSH 1.000000
PUSH 8.000000
PUSH 0.000000
PUSH 0.000000
PUSH 1.082390
FETCH 1
MUL
PUSH 22.500000
PRIM 5
Parse_OK
Beginning GCODE run
Ending GCODE run
Created 371 polygons
Found 0 errors
Partitioning....
Grouping...
Distance testing
MergeCount: 277
tests: 14599
Board boundaries: Rect: [0.162400,0.064700] -> [2.913000,1.577300], w: 2.750600, h: 1.512600
Found 94 groups
lengthdb size 0
DRC space fail: [0x1a0fcd0 0x1a0fd70] 0.005600 - 0.006000
DRC space fail: [0x1a0fd70 0x1a0fcd0] 0.005600 - 0.006000
DRC space fail: [0x1a0fe10 0x1a0feb0] 0.005500 - 0.006000
DRC space fail: [0x1a0feb0 0x1a0fe10] 0.005500 - 0.006000
DRC space fail: [0x1a0feb0 0x1a0ff50] 0.005500 - 0.006000
DRC space fail: [0x1a0ff50 0x1a0feb0] 0.005500 - 0.006000
DRC space fail: [0x1a0ff50 0x1a0fff0] 0.005500 - 0.006000
DRC space fail: [0x1a0fff0 0x1a0ff50] 0.005500 - 0.006000
------------------------------------------------
exit status: 255
DRC put out 33 lines of logging code

the fails I see are:

DRC space fail: [0x1a0fcd0 0x1a0fd70] 0.005600 - 0.006000

DRC space fail: [0x1a0fd70 0x1a0fcd0] 0.005600 - 0.006000

DRC space fail: [0x1a0fe10 0x1a0feb0] 0.005500 - 0.006000

DRC space fail: [0x1a0feb0 0x1a0fe10] 0.005500 - 0.006000

DRC space fail: [0x1a0feb0 0x1a0ff50] 0.005500 - 0.006000

DRC space fail: [0x1a0ff50 0x1a0feb0] 0.005500 - 0.006000

DRC space fail: [0x1a0ff50 0x1a0fff0] 0.005500 - 0.006000

DRC space fail: [0x1a0fff0 0x1a0ff50] 0.005500 - 0.006000

The image they send back, as far as I can tell, has nothing on there to tell me what is wrong

One problem is you’re using BatchPCB. Go to Itead or OSH Park.

The only thing I see is that little IC. What’s the pitch on that IC?

codlink:
One problem is you’re using BatchPCB. Go to Itead or OSH Park.

The only thing I see is that little IC. What’s the pitch on that IC?

Its a Linear LTC 6820 (MSOP16)

MSOP-16 (4.0 x 3.0 mm body width, 0.5 mm pin pitch)