Hello all,
My shiny green boards finally came today. They look almost perfect at a glance, but after careful examination it appeared that all the drill holes are reduced to the same small size, including the 4 stand-offs, which are from spark-fun eagle library.
What did I do wrong? Did any of you all have similar problem?
Thanks!
Here’s the picture of the board:
http://www.batchpcb.com/imgviewer.php?i … b5440e2b3f
Generated by EAGLE CAM Processor 5.0.0
Device : Excellon drill station with user supplied rack file
Parameter settings:
Tolerance Drill + : 0.00 %
Tolerance Drill - : 0.00 %
Rotate : no
Mirror : no
Optimize : yes
Auto fit : yes
OffsetX : 0inch
OffsetY : 0inch
Layers : Drills Holes
Drill File Info:
Data Mode : Absolute
Units : 1/10000 Inch
Drills used:
Code Size used
T03 32.000mil 55
T04 40.000mil 5
T08 130.000mil 4 -------- incorrect drilled
T09 0.600mm 19
T10 0.700mm 8
T13 1.200mm 1
T14 1.800mm 5 ---------------- incorrectly drilled
T15 2.300mm 1 ------------ incorrect drilled
Total number of drills: 98