Eagle files

Why don’t the ATMEGA168 eagle file in the Sparkfun lib not match the ATMEGA168 in the Arduino-Pro-Mini-v10.sch file?

Also, the same file shows the FTDI Basic connector, but it is not in the Sparkfun lib that I could find. However the info shows that it is part of the Sparkfun lib.

They do match and they are both in there… Do you update your EAGLE library? :roll:

(the ATMega168 is called “ATMEGA168” (in the TQFP32-08 package) and the header

is called “ARDUINO_SERIAL_PROGRAMPTH”, both in the schematic editor)

If you can’t find them, why can’t you just copy them?

FartingMonkey92:
They do match and they are both in there… Do you update your EAGLE library? :roll:

(the ATMega168 is called “ATMEGA168” (in the TQFP32-08 package) and the header

is called “ARDUINO_SERIAL_PROGRAMPTH”, both in the schematic editor)

If you can’t find them, why can’t you just copy them?

Ok, Just DLed the Sparkfun lib again, and it has the parts in it.

The odd thing is I just DLed the file a week ago from the same link, but obviously wasn’t the right lib.

thanks.