Hi,
I am using this part and for some reason I am measuring 1.8 kohms between the two pins of the “AC from inverter” input socket. Since I also have a brand new one, that doesn’t show that low a resistance between the two pins, I assume I somehow broke the part.
I had it connected in this way:
I soldered two pins into the holes directly next the AC input, and connected the AC input that way. Then I connected a piece of EL wire to the existing socket, going off the side. Could that have damaged the board?
I am not excluding a mistake, i.e. almost short circuit from soldering, but given that I am measuring a constant 1.8 kohm, I think I can exclude that possibility, can I? Also, the board had been working using this exact configuration, only after using it for some time, the problem started occuring, and I noticed it because all channels would flicker constantly, and/or not lighting up at all anymore, regardless of the input provided on the A-H control pins.
Is there any measurement I could take on the board, besides measuring the pins directly, that would allow me to pin down the issue?