Eliminating the file LOGCON

Hi.

Is possible to program a fixed configuration of Logomatic v.2 eliminating the need to file LOGCON?

I am not able to do so. Someone could help me?

Many thanks!!

OK, I understand that I must change the file main.c, and also where and how to do it to work without the file LOGCON but I wonder why, on the original version of the Logomatic V2, the first file created is called LOF01 (not LOG01) and the other ones LOGxx.

Another question: if I make alwais the same file without checking waht I have on the SD I make only the overwriting of the same file or I have also other problems?

Ok, no answer but did anyway. For your information I have verified that the “LOF01” is a programming error in the original firmware