Errors IDG300 & ADXL335

I don’t know if that going here. :oops:

I have got two sensors, one IDG300 and one ADXL335.

Both are alimented at 3,3V.

I’ve connected Vcc, GND, and the outputs XYZ, but i don’t know why, the circuits don’t work.

I have got a ADXL322 of the robonova, and that sensor works perfectly. Do your sensors need something special to work?, have I to connect another output (Vref,ST?¿)

For example, the output X from the IDG300 is oscillating continuously, but the Y is always at the same value…

Thanks for your time.

ok, the ADXL335 works perfectly, but the IDG300 seems broken :x

I’ll order a new gyro :?