So I’ve finally designed my board, and am trying to get it created. I ran the gerber.cam job/macro, and after adding a new job called Supply AGND, that only has the $AGND layer selected (obviously a ground layer), and telling it to optimize and output with the name *.ly2 (since it is layer 2), it complains about "
!!! APERTURES MISSING - NO PLOTFILE HAS BEEN PRODUCED!"
I told it to emulate apperatures after that, then it only says it once… but i don’t know if that is a workaround, or it just ignores a crucial part of this.
Secondly, I’m trying to use 4pcb.com to make my board, but when i upload my *.drd.#### files (I have two of them, *.drd.0102 and *.drd.0116, presumably for different sizes), the site complains. I use their freedfm part, and select them both as nc drill files, and it complains about having two. What am I supposed to do? Is there a way to make the excellon.cam job compress them into one file, or some other workaround for getting 4pcb.com to work?
EDIT: Okay, i found out they actually mean drills from layer 1 to 2, and layer 1 to 16, but I still need help with how to put up ones 4pcb will accept.
Below is a copy of my GPI file before I added the “emulate appertures” checkbox.
Photoplotter Info File: C:/Program Files/EAGLE-4.16/projects/snrprojsensor/sensor1.gpi
Date : 5/24/2007 12:57:29p
Plotfile : C:/Program Files/EAGLE-4.16/projects/snrprojsensor/sensor1.ly2
Apertures : C:/Program Files/EAGLE-4.16/projects/snrprojsensor/sensor1.whl
Device : Gerber photoplotter
Parameter settings:
Emulate Apertures : no
Emulate Thermal : no
Emulate Annulus : no
Tolerance Draw + : 1.00 %
Tolerance Draw - : 1.00 %
Tolerance Flash + : 1.00 %
Tolerance Flash - : 1.00 %
Rotate : no
Mirror : no
Optimize : yes
Auto fit : yes
OffsetX : 0inch
OffsetY : 0inch
Plotfile Info:
Coordinate Format : 2.4
Coordinate Units : Inch
Data Mode : Absolute
Zero Suppression : None
End Of Block : *
Missing Apertures:
-------- Requested Aperture --------
Shape Size used
thermal 0.0800inch x 0.0600inch 1
annulus 0.0800inch x 0.0000inch 1
annulus 0.0720inch x 0.0000inch 7
thermal 0.0720inch x 0.0520inch 1
annulus 0.0840inch x 0.0000inch 2
thermal 0.0860inch x 0.0660inch 1
annulus 0.0951inch x 0.0000inch 2
annulus 0.0636inch x 0.0000inch 21
thermal 0.0596inch x 0.0396inch 16
Apertures used:
Code Shape Size used
!!! APERTURES MISSING - NO PLOTFILE HAS BEEN PRODUCED!