So I just got the new sparkfun BT module in and replaced the old Mitsumi module with it. It seems to work fine, except I can’t figure out how to get it to go into command mode. With the Mitsumi, I’d connect from my PC and do “+++\n” and it would return “OK”. With this one, I try the same, and I get “+++\n” out the other end. Any subsequent characters are sent straight on through to the other end.
codewrighter:
I’m also having trouble getting into command mode, no idea how to do it. Any help would be appreciated.
Actually I finally figured it out. It appears that you can only enter command mode from the host, that is the device that is connected directly to the BT module. And secondly, a close reading of the datasheet reveals that commands must be terminated with ‘\r’ instead of ‘\n’.
I’m still having a hard time reliably working with it, though, for example trying to change the name of them module or the baud rate. Guess I can try the other new bluetooth module instead… sigh.