Hello,
thanks for great peace of software!
Earlier this year I successfully used OpenOCD for programing external
flash on my LPC2292 board. Flash is TE28F320C3 from INTEL.
Now, I am back to ARM again, and when I install last (SVN88RC2)
version of OpenOCD, and try to program my board I constantly getting
this message (OpenOCD window):
C:\Program Files\openocd-2006re82\bin>openocd-pp -f arm7_wig.cfg
Info: openocd.c:82 main(): Open On-Chip Debugger (2006-08-01 12:00 CEST)
Warning: arm7_9_common.c:675 arm7_9_assert_reset(): srst resets test logic, too
Info: server.c:67 add_connection(): accepted 'telnet' connection from 0
Error: arm7_9_common.c:1910 arm7_9_write_memory(): memory write caused data abort
Error: armv4_5.c:558 armv4_5_run_algorithm(): timeout waiting for algorithm to complete, trying to halt target
Error: arm7_9_common.c:1910 arm7_9_write_memory(): memory write caused data abort
and commands that I sends are:
Open On-Chip Debugger
> flash probe 0
flash 'lpc2000' found at 0x00000000
> flash probe 1
flash 'cfi' found at 0x80000000
> flash protect 1 0 40 off
> flash erase 1 0 40
> flash write 1 linux.bin 0x8000
flash program error
wrote file linux.bin to flash bank 1 at offset 0x00008000 in 29s 218750us
>
I tried on windows and on linux, I get same error on both platform,
with two diferent LPC2292 based boards.
Sometimes, some of location at 0x80008000 and above a successfully
written, sometimes there are no data in flash… everything is
still erased.
please can you help me to resolve this:
this is my config file:
#daemon configuration
telnet_port 4444
gdb_port 3333
#interface
interface parport
parport_port 0x9800
parport_cable wiggler
jtag_speed 7
#use combined on interfaces or targets that can't set TRST/SRST separately
reset_config trst_and_srst srst_pulls_trst
#jtag scan chain
#format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)
jtag_device 4 0x1 0xf 0xe
#target configuration
daemon_startup reset
#target <type> <startup mode>
#target arm7tdmi <reset mode> <chainpos> <endianness> <variant>
target arm7tdmi little run_and_halt 0 arm7tdmi-s_r4
#target_script 0 reset h2294_init.script
run_and_halt_time 0 30
working_area 0 0x40000000 0x40000 nobackup
#flash configuration
flash bank lpc2000 0x0 0x40000 0 0 lpc2000_v1 0 14765 calc_checksum
flash bank cfi 0x80000000 0x400000 2 2 0
and this dump from OpenOCD window when I start it with -d
switch.
http://www.orpid.co.yu/test/dump_flash_error.zip
thanks in advance
Branko Karaklajic