FACET RTK PPP logging icon

Trying to gather 24 hours of data for PPP.

I entered the device via WiFi and menu selected the button labeled, “Reset to Logging Defaults(NMEAx5 + RXMx2)”.

Saved, exited and Restarted. (I did verify that the 2 additional RXM messages are now selected)

The icon on display shows the SD card with the animated logging icon, NOT the SD card icon with a “P” inside of it which I expected.

https://docs.sparkfun.com/SparkFun_RTK_ … _messages/

https://docs.sparkfun.com/SparkFun_RTK_ … /displays/

Am I doing it wrong? Also, I’m in Rover mode…wasn’t sure if it mattered.

Thanks!

Sorry for the confusion! That icon was added in v2.4: https://github.com/sparkfun/SparkFun_RT … s/tag/v2.4 I suspect you are logging correctly but are operating on an older firmware version.

Instructions for updating the firmware are here: https://docs.sparkfun.com/SparkFun_RTK_ … e-from-gui

Perfect! 1. Indeed the data was gathered, and the Canadians did a fabulous job giving me a location. 2. I upgraded to 2.5 and now get the animated P icon. The Windows GUI for the firmware update would not launch on my machine, but I was able to update via the WiFi method.

Thanks for the help!

Excellent! Glad to hear it.