I have my first eagle board attached. Will you take a look and see if I have any glaring errors or if I misunderstood the process in some way? Thank you.
One tutorial on eagle suggested a V+ plane on top of the board and GND plane on the bottom. Sparkfun seems not to use these in some of the boards I have downloaded and viewed. What should I do?
The vreg is an LM1117A and I am expecting it to output 5V. I used the suggest application from the data sheet.
Eagle files are here <old files removed!>
http://www.trailingbit.com/wp-content/u … .14-PM.png
(Power traces increased in size)
I designed this board to hang on the back of a 4x20 LCD connected by the 16 pin header. That is why I didn’t add standoffs. The dimensions are 2.3 x 2.45. I am hoping to match the footprint of the LCD, but I might need some minor adjustments. I still need to do a 1:1 test print, but I am waiting for the surface mount components to arrive.