I think I’m ready to submit it to BatchPCB–kinda scary. It has two independent batteries and solar chargers; then a DC/DC booster; and an “emergency” (4) AA battery pack in case every thing else quits working. The goal is to create a 5V power supply that’s pretty redundant and can reliably deliver 1A.
Thank you. I was worried about the power tracks. I’ll try to fatten them up. I’m curious, why are 90 degree corners bad. Are the tracks likely to break up at that point during etching?
Depending on the manufacturer sometimes you get “acid traps” at 90 degree bends. You really only need to avoid 90 degree bends when you get into higher frequencies; however, I just find it better to be safe than sorry.