Cralis:
Thanks for that!
Been looking at the forums and links. There seems to be a very good, 500 line Sony 3cm by 3cm camera for around US$70… I can’t recall the model, but it seems to get pretty good reviews, and they rekon it’s comparible to a DVD quality image. Mmm…
None of these cameras will be DVD quality, post up that one you are talking about, chances are I will know a bit about it. There isn't too many different cameras in use for FPV.
Cralis:
I’m pretty down about the DX7 issue though. I was hoping to start off with a static mount, and then upgrade to pan and tilt. The benefit would be ‘sale0ability to my wife’. I’ve told her that if I buy it, she could wear the goggle sometimes, and I can fly like normal RC… and she can look about. That would be pretty amazing, and she’s pretty keen!
So - options. Replace the DX7 with a different 2.4Ghz system? (I’d like to stay with 2.4 - as my other aircraft all run AR7000s and AR6100s. Is there no module you can get to add to the aircraft? Another ‘pan and tilt’ Tx and another Rx on the aircraft?
It's complicated... (Isn't it always?)
The problem comes from the DX7 not mapping the the aux channels to the trainer port, where the head tracker (HT) normally injects its data. I know guys who are using the DX7 as “master” TX and using another radio linked to that as the actual controller, with the HT injecting into the slave. I have never really bothered with HT’s so I would have to look into it a bit more to know what your options are.
Cralis:
How did you manage to get the radio equipment for $100? I really like the look and flight charactoristics of the Easy Glider. What’s the difference between the EasyGlider and the Easy Glider Pro? And replacement part availability? Seems to Pro is the newer version - But around $50 more.
Radio gear? Difference is the Pro is the new version that has brushless mounts, don't even think of getting the old one. If by radio gear you mean the motor+esc I will post some links further down.
Cralis:
The extra small costs not included would be: Lipo? (Maybe a 3S 1000mah - I belive that gives you around 50 minutes) Cables? Lens?
1000mah is WAY to small. I run a 2400mAH in my EagyGlider but am thinking of upgrading to a 3600mah or thereabouts.
Cralis:
I’m building a spreadsheet of parts - and taken your advice and focusing on the 900Mhz goodies. What is the difference between 900 and 1.3? Image quality the same - just slightly longer range on 900? The thing is, it’s just the Rx and Tx that make the system 900mhz, right? So, if the day came that I wanted to go 1.3 - it’s a case of replacing just the Rx and Tx - not the MOST expensive parts in the whole system…
Yes it's just the TX and RX that are to do with the frequency. The most expensive part is the goggles.
Cralis:
These Rvision-D high resolution goggles. Are their better, equal or worse alternatives? And can the video be recorded pretty easily to an SD card or something, somehow?
They are the best without getting stupid. I own them as well as some Fatsharks. I like both but the fatsharks look more cool. They are more $$$ though. Then there is the Headplay ones, which are something stupid like $500... They are (apparently) the best, but you pay for it.
Cralis:
Also - did you source your aircraft locally? It seems it’s better to buy from the US - but postage can make you weap a bit. 
I was impatitent when I got my EZGlider, I got it from the North Coast for $150 posted... Retail was only $120 though, a very good price.
AndyL:
It does change one thing, In some nations (Like USA) 1.3ghz is reserved for “AERONAUTICAL RADIONAVIGATION” according to my FCC frequency allocation chart. I assume in Australia this isn’t a problem?
It is not quite as clear cut as that, but I
**am not** going to go into that here.
Cralis:
Not sure - I’ll look into it.
I agree about the costs - but … I fear it’s all going to add up, and we’ll have around a grand of electronics up there. Time to look into the availability of an emergency parachute! 
Don't bother looking into it, you won't find any answers, trust me. PM me if you are really interested though. It's a whole new rant/thread in itself.
You shouldn’t have a grands worth of gear airborne, at most you have a $250 airplane, just like any other RC airplane, then you have $200 worth of video gear on it. The big cost is goggles really.
Cralis:
Gussy - I have a suppier who can get me an Easy Glider PRO for $120… or the Easy Glider for $100. He says the only difference is that the PRO comes with a Brushless mount… Which, I guess is the way to go for the extra weight and wind resistance offered by FPV?
Edit: Answered one of my questions.
Differences between EasyGlider Pro and Easy Glider Electric:
(snip)
As I said above, go for the $120 one. MPX stuff is excellent value.
Cralis:
I’m trying to build up a list of items for the Easy Glider, and this is what I have at the moment.(snip)
Ok this is what you want. The best setup.
Ditch those HS55 servos, unless you have them laying around. The HXT900’s are just as good, if not better, and $3.
ESC: [Turnigy Plush 40A ESC
Outrunner: [TGY AerodriveXp SK Series 35-30 1100Kv / 345w
Aileron Servos: 2 x [HXT900 9g
Elevator + Rudder Servos: 2 x [Hextronik MG-14 14g
LiPo: 2350mAh 3S (20-25C)
Prop: [TGS 11x8F Precision Folding propeller
Spinner: [Folding Prop Spinner 45mm / 4.0mm shaft
There are plenty of options for LiPo’s, I am running [these at the moment, but thinking of upgrading to something bigger soon. They will get you going though if you don’t want to make a decision. Great value too at $19, grab a few.
I think I covered everything… if not, let me know.](http://www.hobbycity.com/hobbycity/store/uh_viewItem.asp?idProduct=7468)](http://www.hobbycity.com/hobbycity/store/uh_viewItem.asp?idProduct=5565)](http://www.hobbycity.com/hobbycity/store/uh_viewItem.asp?idProduct=7985)](http://www.hobbycity.com/hobbycity/store/uh_viewItem.asp?idProduct=8303)](http://www.hobbycity.com/hobbycity/store/uh_viewItem.asp?idProduct=662)](http://www.hobbycity.com/hobbycity/store/uh_viewItem.asp?idProduct=7075)](http://www.hobbycity.com/hobbycity/store/uh_viewItem.asp?idProduct=2165)