This is my first board. Can someone please check this board before I send it off? Thanks.
Attachment doesn’t work.
I have edited the post and re-attached the attachement. Thanks.
Its a Xport socket and a connector, how wrong can it be? lol
If I was to say anything then…
I’d make the connections as thick as you can where they exit the connectors, this is because when plugging in/unplugging them you stress them and they can rock causing thin tracks to break at the point where they enter the pad. It is common to add what is called a teardrop (triangle of copper) at this point.
Another method is to simply exit with a thick track, necking it down 1/2" away from the pad.
But that’s likely going way over the top for this little board.
Or make absolutely sure that your drill holes are all the correct metric size, especially for the Xport locating pins.
Thank you for your feedback. I realize that it might be a very simple board but this is my first board and I have not done one so I just wanted to be sure that I didn’t leave anything aside.