FIX: ATmega128RFA1 ARDUINO ADDON

Following the ATmega128RFA1 Dev Board Hookup Guide https://learn.sparkfun.com/tutorials/at … okup-guide. When adding the board hardware files (platform.txt, board.txt, etc) arduino produce the following errors while uploading through FTDI using avrdude.

Warning: platform.txt from core 'SparkFun AVR Boards' contains deprecated compiler.path={runtime.ide.path}/hardware/tools/avr/bin/, automatically converted to compiler.path={runtime.tools.avr-gcc.path}/bin/. Consider upgrading this core.
Warning: platform.txt from core 'SparkFun AVR Boards' contains deprecated tools.avrdude.cmd.path={runtime.ide.path}/hardware/tools/avr/bin/avrdude, automatically converted to tools.avrdude.cmd.path={path}/bin/avrdude. Consider upgrading this core.
Warning: platform.txt from core 'SparkFun AVR Boards' contains deprecated tools.avrdude.config.path={runtime.ide.path}/hardware/tools/avr/etc/avrdude.conf, automatically converted to tools.avrdude.config.path={path}/etc/avrdude.conf. Consider upgrading this core.
Warning: platform.txt from core 'SparkFun AVR Boards' contains deprecated recipe.ar.pattern="{compiler.path}{compiler.ar.cmd}" {compiler.ar.flags} {compiler.ar.extra_flags} "{build.path}/{archive_file}" "{object_file}", automatically converted to recipe.ar.pattern="{compiler.path}{compiler.ar.cmd}" {compiler.ar.flags} {compiler.ar.extra_flags} "{archive_file_path}" "{object_file}". Consider upgrading this core.
Bootloader file specified but missing: /home/garza/Arduino/hardware/sparkfun/avr/bootloaders/atmega/ATmegaBOOT_168_atmega128rfa1.hex

Sketch uses 712 bytes (0%) of program storage space. Maximum is 126,976 bytes.
Global variables use 9 bytes (0%) of dynamic memory, leaving 16,375 bytes for local variables. Maximum is 16,384 bytes.
java.io.IOException: Cannot run program "{path}/bin/avrdude": error=2, No such file or directory
	at java.lang.ProcessBuilder.start(ProcessBuilder.java:1048)
	at java.lang.Runtime.exec(Runtime.java:620)
	at java.lang.Runtime.exec(Runtime.java:485)
	at processing.app.helpers.ProcessUtils.exec(ProcessUtils.java:11)
	at cc.arduino.packages.Uploader.executeUploadCommand(Uploader.java:123)
	at cc.arduino.packages.uploaders.SerialUploader.uploadUsingPreferences(SerialUploader.java:167)
	at cc.arduino.UploaderUtils.upload(UploaderUtils.java:78)
	at processing.app.Sketch.upload(Sketch.java:1178)
	at processing.app.Sketch.exportApplet(Sketch.java:1152)
	at processing.app.Sketch.exportApplet(Sketch.java:1124)
	at processing.app.Editor$DefaultExportHandler.run(Editor.java:2430)
	at java.lang.Thread.run(Thread.java:745)
Caused by: java.io.IOException: error=2, No such file or directory
	at java.lang.UNIXProcess.forkAndExec(Native Method)
	at java.lang.UNIXProcess.<init>(UNIXProcess.java:248)
	at java.lang.ProcessImpl.start(ProcessImpl.java:134)
	at java.lang.ProcessBuilder.start(ProcessBuilder.java:1029)
	... 11 more

This is for recent IDE versions of arduino ( 1.6.6, 1.6.7 and 1.6.8 ), because arduino changed some compiling settings.

This was solved changing the platform.txt and boards.txt as follows

boards.txt

https://gist.github.com/Guardado/11871c … 8a51cbc335

platform.txt

https://gist.github.com/Guardado/e344df … 0d5c6e0bfe