This isn’t about sparkfun stuff, but you guys were helpful in the past about my arduino and other components I did order from sparkfun in the past, so I thought I’d put this here. If its the wrong forum, I apologize.
I bought a cheap Chinese LED light for my aquarium 2y ago and it failed. After pulling it apart it seems that each led (there’s around 50 across two ‘circuits’ soldered to an aluminum pcb) has a diode in parallel with it. It looks like a small SMD glass zener diode with an orange and blue end. A few have burnt out and shorted which I’m guess is the reason for the lights failure. The leds are powered by a proper constant current AC to DC power supply, so I’m not sure why the diodes would be necessary.
Should I just desolder/remove the burnt/broken ones? Will this cause the others (or the LEDs or the drivers) to fail quicker? Should I try to replace them and if so, how do I find out which ones I would use? TBH I’m not entirely sure why they are even there so I have no clue which diodes I would order to replace them, or how necessary they even are. Given that the whole thing is powered by a constant current dc power supply it seems there would be little need for the diodes. Any ideas?