Hello everyone ,
I am new to openocd .
I am using Atmel SAMD21 xpro board .My host system is Ubuntu LTS 14.04.1
When I am using make flash command , I get follwoing error.
flash write_image erase /home/pinkesh/RIOT/RIOT/examples/samd21_default/bin/samr21-xpro/default.hex: command requires more arguments
in procedure ‘flash’
make: *** Error 1
Open On-Chip Debugger 0.8.0-dev-00175-g8b7acca (2014-10-15-16:59)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : only one transport option; autoselect ‘cmsis-dap’
Info : CMSIS-DAP: SWD Supported
Info : CMSIS-DAP: Interface Initialised (SWD)
adapter speed: 500 kHz
adapter_nsrst_delay: 100
cortex_m reset_config sysresetreq
Info : CMSIS-DAP: FW Version = 01.1B.00FC
Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 1 TDO = 1 nTRST = 0 nRESET = 1
Info : DAP_SWJ Sequence (reset: 50+ ‘1’ followed by 0)
Info : CMSIS-DAP: Interface ready
Info : clock speed 500 kHz
Info : IDCODE 0x0bc11477
Info : at91samd21j18.cpu: hardware has 4 breakpoints, 2 watchpoints
TargetName Type Endian TapName State
0* at91samd21j18.cpu cortex_m little at91samd21j18.cpu halted
target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x00000300 msp: 0x20002980
target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x00000300 msp: 0x20002980
flash write_image erase /home/pinkesh/RIOT/RIOT/examples/samd21_default/bin/samr21-xpro/default.hex: command requires more arguments
in procedure ‘flash’
make: *** Error 1[/img]