fv-m8

hi all!

1.how should i interface fv-m8 with pc, what all i need to buy along with fv-m8 to get the data displayed in minigps or gps locator utility. circuit diagram is appreciated.

2.i am using avr atmega8 microcontroller for extracting data from fv-m8 and display the contents on lcd. i need help in what all components to be used here along with fv-m8. circuit diagram is appreciated. reply asap.

You will need a power supply and a RS232 chip.

Hi,

I have a Question ???

I am a student and i m using GPS 32 channel san jose navigation module and GPS Evaluation Board GPS-08334 for data extraction .

When i use USB interface of Evaluation board (GPS-08334) for data extraction it will work…

But unfortunately when i want to use uart interface of evaluation board it is not workng…

Do you have any suggesstions…

Power supply and FT232 cable (USB to TTL-serial).

Waqar, if you connect only the RS232 cable, the module will not be powered. Keep the USB cable connected, even if communication is done through RS232 DB9 connector.

Angelo

Thanks Angelo for reply…

I have tested but it is not working…

Do you have some other solution…