I have tried to change the I2C address on one of two Lidar modules I have on this Arduino project. However, I always get a Nack in response. And then both give the same distance, even when I place a card in front of one of them. Has anyone had success in changing the address? I have tried several addresses like 0x63, 0x64, 0x65, 0x66 as well, to no avail. I have tried the two libraries (Lite and Litev3HP) with the same result. I also tried to use one in PWM mode, but due to timing issues, those distances are very large and inaccurate.
Try running through the steps on pages 4 and 5 here https://cdn.sparkfun.com/assets/9/a/6/a … ations.pdf - you have to have the unit ‘talk to itself’ (loopback serial number of device) before you can change the address ![]()
The library calls to setI2Caddr does this ‘talk to itself’ process–this is true of both library versions. If I do this with only one Lidar attached, that works, However as soon as I power off the unit, the original address is back in play. Power cycling is very typical during development, so hard to avoid, having the base address return. Of course what I need is to have 2 of these units attached, so then applying a new address does not seem to work. Is there anyway to have the address change “stick”, so that power cycles do not affect it?