I put a newly formatted flash into the GeoChron, turned it on for a few minutes, turned it off, and removed the flash.
After inserting the flash in my Windows XP computer, I edited the GLOGCON.TXT file, as follows:
Mode = 2
Log What = RMC
Time Between Logs = 00:00:00
Holdoff = 15
WAAS = 0
Bluetooth Active = 0
I saved the file, removed the flash, and installed back it into the GeoChron.
With the GeoChron attached to power and the standby switch in the run position, I turned on the device and let it run for a few minutes.
I removed power and waited for the LED to go dark.
Putting the flash back in my computer, there were no files visable.
Disk properties show that 96k of the disk is used, but I cannot see the files.
Any idea what is going on?
Version information from the LOG0.tst file prior to the GLOGCON.TXT file modification:
$PSRFTXT,Version:GSW3.2.4_3.1.00.12-SDK003P1.00a
$PSRFTXT,Version2:F-GPS-03-0701301