Hello,
We recently purchased several GPS-08334 evaluation boards with one USB connection and two serial connections.
Eval Board:
http://www.sparkfun.com/commerce/produc … ts_id=8334
GPS:
http://www.robotshop.us/lassen-iq-gps-receiver.html
We have installed the FTDI driver for Windows XP (which we are using) using the executable on the FTDI website. The coin battery is in, the USB/RS232 switch is set to RS232, and the other switch is set to Int. Not sure exactly what these do.
The unit is being powered externally, the red light is on, and a couple of seconds after turning the power switch to ON, the green status light is lit. Port 1 of the eval board is plugged into Port1 of the PC.
I am using TrimbleMon_V1-05-0.exe to connect to the unit. When I use Initialize > Detect Receiver, it detects nothing (even if all check boxes are checked – trying everything). However, I can connect to the board using Initialize > Connect using 9600-8N1 or 9600-8O1, but 9600-8O1 I think is default.
After manually connecting and with an antenna connected, I can see satellites and download the complete almanac. However, none of the satellite information is shown on the right half of the screen, and no version information is shown on the bottom of the screen. All other fields are filled in with time/position data. Further, when I go to configure the receiver, none of the options are filled it and I cannot change any of them. When I click Query on any tab, nothing happens.
I also tried Trimble GPS Studio and get the same thing. I also tried iQ_CHAT to change port settings, baud rates, etc, and nothing changes when I try to write it to NVM (“…waiting for reply”). I tried using the USB connection to do all of the same things, and the same things happen. I feel like I have literally tried everything.
As a note, when I first install the FTDI driver for the USB connection, I don’t see two COM ports show up (the lower for Port 1, the higher for Port 2). Is this all a driver problem? I have installed the driver several times. I have tried this on multiple computers. All boards we have are behaving the same way, so it doesn’t seem like it is a board problem.
Could someone please walk me through what I could be doing wrong, or what I need to do to get this to work? Hopefully the fact that I can connect and download almanac, but the configuration is not filled in or changeable, is something that indicates what the issue is.
Thank you all in advance for your help.