GPS P2 signal for RTK Surveyor

Hello,

I’m testing the RTK Surveyor logging RAWX and SFRBX data. I collected a GPS test data set and converted the UBX to RINEX 2.11 successfully, but an issue has popped up. My test file contains signals C1, L1 and L2, but not P2.

Is there any setting in the ublox chip i can change in order to get P2 signal?

Thanks in advance

The ZED-F9P supports L1C/A and L2C. I don’t believe it supports P2. See attached image from the ZED-F9P-02B datasheet (https://content.u-blox.com/sites/defaul … 023276.pdf).

ZED-F9P signals.jpg

Thanks for the reply.

We know P2 signal is required for NOAA Antenna Calibration, so how could Sparkfun RTK Facet success the NOAA calibration?

Thanks

P2 is not required to my knowledge. Please link to a resource where this is stated as required.

These are the tracking Capabilities selected when we applied for the RTK Facet certification: GPS L1/L2/L2C, GLONASS L1/L2, B1/B2/B3, E1/E5b

Got it, we would made a mistake when applying for certification if they are asking for P2 signals.

Thanks for your help