I have adquiered a MG-S01SP GPS module wich come with an internal antenna… I’ve just finnish my SCH now I’m moving on the PCB… Should I have any consideration about it?
I was planning to use a connector so it is a little elevated from the board, so I can gain some more space on it… Should I do that? Obviously the chip Antenna would be on top…
Most GPS antennas like larger ground planes underneath them. The effect of such a ground plane with the antenna mounted high up on another board assembly won’t be as great however.
I’m back with a new question… Now it’s because I want to reduce some space…
Besides the GPS I have a GSM/GPRS MODULE, wich I only use to transmit data via GPRS and send SMS, but no AUDIO…
I’m doing a double layer PCB. I was planning to place the GPS in the bottom layer with its ground plane in the same layer… And in the top layer i want to place the GSM/GPRS, at the same level, with a ground plane for it in the top layer… Did you understand what I mean? In one side is the GPS and in the other, the GPRS…
The short answer is no. A ground plane isn’t a brick wall to RF signals (especially on a 2 layer board, it’s not even really a plane - it just fills the gaps between the traces). The fibreglass that makes up the bulk of the PCB acts like a capacitor at GPS/GSM frequencies - that’s why most antennas call for a ‘50 ohm microstrip’ where the ohms measures complex impedance, not resistance.
Could i ask you too about where to shop this modules, a direct dealer? are this modules available in small quantities? I can’t find this on arrow, mouser nor digikey.
I see you are from Chile, so… porque no hablamos español? jeje
Yo los consigo a travez de la empresa donde trabajo, y ellos se los compran a CIKA http://www.cika.com.ar/. No sabría decirte el precio del SIM340DZ, se que el SIM340 sale alrededor de 70 dolares, y el DZ es un poquito mas caro, pero no se bien cuanto xq todavia no lo compre…
No conozco de otro distribuido o empresa que los venda… Esta es la pagina del fabricante http://www.sim.com/, tal vez la puedas conseguir a traves de ellos… No se que si tendran cantidades minimas…
Respecto a CIKA, no utilices su buscador, porque no lo actualizan desde el 2004, mejor envia un mail y pregunta… Supongo que manejan cantidades pequeñas.
Espero haber contestado tu pregunta… De todos modos, te sugiero que crees un nuevo tema en el foro y ahi preguntes por lo mismo, porque la gente de aca es muy buena onda, y de seguro sabran responderte… Y de paso no se mezclan los temas… Cualquier duda avisame, por aca o mandame un mensaje privado