I have hooked up the receiver and have it connected to a macbook. I used the a USB MB5 as the converter. I get data and it seems just like nothing of value other then it looks like the correct format.
this is all I get out of it:
$GPRMC,V,N*53
$GPVTG,N*30
$GPGGA,0,00,99.99,*48
$GPGSA,A,1,99.99,99.99,99.99*30
$GPGSV,1,1,00*79
$GPGLL,V,N*64
this would tell me the GPS radio either does not work is not connected properly, or is not seeing anything.
Do I have to set it up with prior to using it?
anybody have any ideas of what diagnostic tools I could use on the Mac?
is the MB5 the wrong thing? If so what should I use?
Thanks anyone…