I was using the H-JTAG Server with the wiggler and the LPC2138 header-board. I had set nTRST to Pin6 and unchecked “nTRST output inverted”. Everything was working, and I’ve successfully loaded multiple programs to flash.
Yesterday I unplugged my laptop from the LPT port, sat back programming, and when I put the laptop back on the table and replugged the lpt port wiggler in, H-JTAG server will no longer connect!
Is there some software setting that could have gotten messed up? Or do you think that I have fried a pin on the header board / MCU?
I’m considering trying to use the Sill boot-loader through serial? The last programmed program is still outputting correctly to the serial port, so at least the whole board is not dead…
http://water.cse.unsw.edu.au/esdk/sill.html
btw, the H-JTAG LPT port test fails… I’m not sure if it failed or not when everything worked?
Thanks for any advice,