HAS/E6 results on PostCard FW V3.1 with LG290P FW V2.01 [Feb 2026]

Elevations are tricky to evaluate in this scenario. The positions were all on a concrete slab, but there was an actual elevation change of 1cm+ according to the RTK positions. From the dataset, there appears to be a 60cm difference in the vertical datums between HAS and PointPerfect Solutions at this specific area (expected).

Once that Vertical Shift is removed between the 2 correction systems, we get the following Vertical Comparison between HAS and PointPerfect:

:bullseye: Vertical Residuals using fixed +60cm elevation bias between datums (Each pair, in cm)

  • -29.53
  • -6.95
  • -5.98
  • -4.96
  • +3.46
  • +4.72
  • +2.39
  • +2.58
  • -1.08
  • -1.11

That’s probably a perfect example of how multi-path influences Elevations more than X and Y. The HAS Elevations tighten-up significantly as we move away from the building, even with a choke ring antenna.

I understand these results are a lot better than the HAS service can technically provide…but it’s an honest test. I do not have an explanation. The same test might produce worse results in the future under different conditions.