Hello I need some help, I am looking for a GPS, for using it at Jalisco, México.
I need to make a topographic survey, for measuring levels and polygonal as mucha as 7 km Diameter.
I have an existing GPS Coordinates point, marked in the ground, with the corrected coordinates, this is an existing rectified coordinate.
There is no Internet at the location.
I need a gps equip with the next capabilities:
A) I need an equip with Base and Rover, RTK.
B) I need to place de Base above the physical existing marked point, which I know the actual coordinates.
C) Fix / Correct the Base coordinates to the real ones.
D) Make the survey with the Rover, RTK. the better precision the best.
E) Save the survey coordinates into a .txt file, or a file which I can handle the coordinates.
I am thinking of the next models:
- GPS-18443 x 2 SparkFun RTK Surveyor
2) (GPS-17751 x 2) GNSS Multi-Band L1/L2 Surveying Antenna - TNC
-
WRL-20029 x 2 - SparkFun LoRaSerial Kit - 915MHz (Enclosed) or WRL-19032 - SiK Telemetry Radio V3 - 915MHz, 100mW ?
-
LoRa Fiberglass Antenna Type N - 5.8dBi (863-870MHz), Can I use this Antena Simultaneously with the Sparkfun RTK surveyor
?
Does this arrangement will be usefull for my needs, or do I need something else to make it work properly?